When does the MQ turn on?

The MQ is equipped with both an internal flow switch and an external pressure switch. Both are able to switch on the MQ when water is extracted. The pump starts up when

the flow rate is greater than 0.07 m³/h


the pressure is less than 2 bar.