Find case

Reset search
Showing 21 to 30 of 47 results
Case banner
Grundfos fire protection system protects shoppers’ paradise in Portugal
Portugal, Alcochete: Freeport Designer Outlet Lisboa officially opened on September 2004, offering over 200 retail outlets, 40 restaurants and cafés, and extensive leisure facilities including a 21-screen multiplex cinema and an amphitheatre with weekly live entertainment. Unlike traditional shopping centres or malls, Freeport is an open-air environment that resembles a village packed with designer shops, selling surplus stock at reduced prices.
Grundfos sanitary range at Jacobsen’s Brewhouse
The kettles at The Jacobsen’s Brewhouse on the Carlsberg property in Copenhagen are brewing specialty beer as ever before. Over the past couple of years, the beer market has taken a U-turn and consumers increasingly demand beer of a quality that reflects old taste and tradition.
High ambitions for Moscow’s Tower 2000
The prestigious Moscow City project covers 100 hectares in Moscow’s central business district, and is due to be completed in 2010. Often described as Moscow’s first “smart building”, the 34-storey Tower 2000 complex contains offices, retail stores, restaurants, underground parking and an observation platform that provides spectacular views of the city.
High pressure pump for RO plant
Weil Industrieanlagen GmbH is a specialist in water purification and water treatment and was established in 1986. The water purification and water treatment techniques both use membrane technology, (reverse osmosis, nano-filtration, and micro-filtration). The company focuses mainly on three technology areas: building technology, energy technology and pharmaceutical and medical technology.
Submersible pumps for vacuum filtration
This useful installation concept from the Bürener Maschinenfabrik (bmf) has already won over several companies in the machine tool industry: the integration of a coil-type suction filter directly in the coolant tank means that the overall coolant conditioning equipment is very compact, with the purification tank no longer required. One of the main components of the concept is a modified immersible pump from Grundfos.
Supreme hotel relies on supreme water disinfection by Grundfos
The biggest 5-star hotel in Sofia disinfects water with Grundfos dosing and disinfection systems.
A fresh start
Battered by decades of war, poverty and a queasy political situation, the challenges facing Afghanistan are immense. Fortunately, assistance is pouring in from all over the globe.
Astramatic: Grundfos pumps in 1,000 m3/day RO plant in Algeria
Astramatic S.A., Barcelona, Spain, is an engineering and consulting company that designs, builds, manufactures, and maintains industrial process water treatment plants adapted to all needs and situations.
Austrian utility: 'We didn't believe energy savings of this size were possible'
For the water booster supply application after sand filtration/backwash at Wasserverband Südliches Burgenland in Oberwart, Austria, Grundfos supplied a CR-95 22 kW model from its new line of
District heating plant tests new Grundfos CR pumps, gains 10 percent efficiency
In autumn 2015, the Danish Hirtshals District Heating plant installed three CR-95 field test units from the new generation of CR multistage pumps. The plant installed two pumps at a waste incineration plant 19 kilometres away in Hjørring, and one at the halfway point on the heating transmission line in Tornby.