FAQ

Showing 51 to 60 of 88 results

During frost periods, users often fail to ensure that the pumped medium is drained completely from the pump chambers.

Read more...

The pumped medium must be completely drained from the pump chambers.

Read more...

If the pump is operating too far to left on the curve, this simply means that the pump is delivering high pressure but at a flow rate that is low or non-existent.

Read more...

When a pump operates too far to the right on the curve, this simply means that the pump is delivering a flow rate greater than that for which it was designed.

Read more...

Unless specified to the contrary, the curves in the Grundfos documentation are specified for the density and viscosity of water at a temperature of 20°C (specific gravity = 1 and viscosity = 1).

Read more...

A cooling jacket, also referred to as a flow generator, ensures that there is always sufficient water flow across the motor surface in order to cool the motor.

Read more...

In a dry-running pump, the component that comes into contact with the medium (the wetted part) is separate from the motor.

Read more...

The pump's input power is the pump's power requirement under the present operating conditions.

Read more...

The NPSH curve displays the minimum required inlet pressure (expressed in m) allowing the pump to pump in accordance with the performance curve and in order to prevent evaporation of the pumped fluid so as to avoid cavitation inside the pump.

Read more...