FAQ

Showing 21 to 30 of 88 results

The float switch cable is to be attached to the discharge pipe in such a way that the remaining free cable length ensures a sufficient flow volume.

Read more...

The dry running alarm is triggered if the motor is running and the flow rate is less than 0.07 m³/h and the pressure is lower than the pressure set on the pressure switch.

Read more...

The dynamic total delivery head is also referred to as the

Read more...

The number of switching cycles is unlimited, as the SQ/SQE is equipped with soft start integrated into the motor.

Read more...

A: Circulator pumps are generally used to circulate hot water. The temperature of the pumped medium is transferred to the pump, and it is normal for the pump's surface to be warm or even hot.

Read more...

Dry running of the pump can damage the mechanical seal and the motor.

Read more...

Yes, that is possible. To do so, connect one phase and the neutral conductor. The voltage between phase and neutral is 230 V.

Read more...

In order to increase the service life of both pump and motor, weather protection should always be provided.

Read more...