FAQ

Showing 1 to 10 of 88 results

Grundfos offers numerous speed-controlled pumps that are referred to as ‘E-pumps’ and which come equipped with Grundfos MGE motors with an integrated frequency converter.

Read more...

SP submersible pumps with a Grundfos or other submersible motor can be operated in any position from horizontal to vertical.

Read more...

If excess temperature protection is not properly connected or bridged, the pump may be permanently damaged.

Read more...

Yes, the pump has an integrated soft start feature in order to reduce start-up current, thus assuring even, continuous acceleration.

Read more...

In the event of a fault, the SQ will perform an unlimited number of restart attempts.

Read more...

In order to protect against frost damage during transport and storage, SP pumps are protected by a water/glycol mixture.

Read more...

VDI Guideline 2035 Part 1 has been in effect since 2005, and VDI Guideline 2035 Part 2 has been in effect since 2009.

Read more...